7/19/2019 6:39 PM | |
Joined: 12/20/2018 Last visit: 1/20/2024 Posts: 63 Rating: (0) |
Hi everybody. (I am inexperienced) I have 331-7KB00-0AB0 Analog module. [snip] And I Have ifm PN5020 Pressure Sensor. How to connect 4-pin cable to analog module and How to measure pressure. Configuration: [snip] |
Last edited by: Jen_Moderator at: 07/22/2019 08:09:28Removed links, because not functional. |
|
7/19/2019 9:35 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Please look at Chapter 6.8 https://support.industry.siemens.com/cs/attachments/8859629/s7300_module_data_manual_en-US_en-US.pdf Is 7KB02 because is the successor of your 7KB00 Attachments7300_module_data_manual_en-US_en-US.pdf (190 Downloads) |
Last edited by: Jen_Moderator at: 07/22/2019 08:11:17Added PDF as an attachment. Removed links from quote. |
|
7/19/2019 9:41 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684)
|
Hello avatar; First point, I have no access to your files, see the attachment below. Next point: from the documentation I can obtain from ifm, the PN5020 is a pressure sensor that give you a digital output (24 VDC) when it reaches a pressure setpoint that you set through the display/menu of the unit. https://www.ifm.com/in/en/product/PN5020 https://www.ifm.com/mounting/701588DEFRUK.pdf From what I can gather you cannot connect it to an analog module, in the hopes of reading a continuous range of pressure.. You connect power (24 VDC) between terminals 1 and 3 (Brown and Blue wires, check your polarity). You connect to the digital input channel with terminals 4 and 3 (Black and Blue wires). Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
7/30/2019 7:59 AM | |
Posts: 5 Rating: (2) |
Come on, it's just a pressure switch, you cannot wire it with analog module... |
Follow us on