11/15/2018 3:27 AM | |
Joined: 7/5/2013 Last visit: 9/19/2024 Posts: 3112 Rating: (512) |
Hello skullcity,
>> 1 record/tag * 5 tags * 12 1/min * 60 min/h * 36 h = 129600 records In a post in the German forum I found a link (WinCC V13 SP1) where you can find the "Number of entries per log (including all log segments)" which is maximum 50000. There was warning when I compiled it with 129600, but maybe better to use one archive per tag.
See the following description:
Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to2 thankful Users |
Follow us on