7/22/2019 3:11 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1643)
|
Hello check the Option+ Package there is a Simatic Logon Basic included. Its the only Way I know for a direct access to the Panel. https://support.industry.siemens.com/cs/de/en/view/109754400 Of course you can use a Profinet or DP or serial Device communicating with the PLC then you can use the Job Mailbox in the HMI connection or you can use a Tag Tigger for the Login from the PLC. but we have to less information to write a reliable soultion suggestion. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
7/23/2019 8:48 AM | |
Joined: 11/19/2018 Last visit: 4/24/2024 Posts: 12 Rating: (1) |
thank you Murof i will check this and get back to u |
Follow us on