7/22/2019 5:18 PM | |
Posts: 1 Rating: (0) |
Hello everyone! I woul like to ask a little help regarding the problem our Siemens 6AV2 123-2GB03-0AX0. The start button is not responsive and we're unable to access the parameter setup. Also we tried the reboot process using USB but the HMI is not reading the external drive. Only Profinet is the only open channel available even with the USB inserted in the port. Hoping for any support regarding this matter. Thanks and regards! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/23/2019 08:00:45New subject after splitting |
|
7/29/2019 1:55 PM | |
Joined: 8/3/2009 Last visit: 4/24/2024 Posts: 12854 Rating: (1639)
|
Hello the transfer mode is running so this is a good thing then you do not have "locked out". do you know the IP Adress of the PAnel? can do you do a Ping to the panel from your TIA Portal Computer? if yes then you can transfer as usual. If you do not see the Panel and you cannot get into the settings (because of password) then you can also do a reset to factory settings and after that you can set the panel and do a project transfer again: https://support.industry.siemens.com/cs/ww/en/view/109744950 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on