7/16/2019 2:24 PM | |
Joined: 6/9/2016 Last visit: 9/12/2024 Posts: 4 Rating: (0) |
Hi! Can you help me with choosing right gearbox for application? I need to choose gearmotor for winder application. I've calculated with the help of SIZER, that my maximum output speed should be about 720 rpm. SIZER proposed to me gearmotor 1FG1106-1QD26-2AF1-Z (I clicked the button "Determine optimum motor"). The thing is N2MAX for this motor is only 529 RPM. Sizer help says, that this is "Maximum gearbox output speed". How is it possible? Sizer proposed wrong motor for me? Or did I understand something wrong? What will happen if this gearbox will work with speed that exceeds N2MAX? Should I only choose motors with N2MAX > maximum calculated speed? AttachmentWinder.zip (271 Downloads) |
Follow us on