7/23/2019 8:38 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
Hi draacula, as I know MODBUS doesn't support timestamp data by itself. But of course you can put a timestamp in any register to be read by the DCS / SER, but this is application specific and not a MODBUS feature. |
iba AG - Data Acquisition and Analysis the way it should be |
|
7/24/2019 8:27 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
Hi draacula, the only place where it could be, is the instance datablock of the ALARM_8P or whatever block you use. But I can't see anything there. I guess it is not possible to "copy" the sent data from ALARM_8P and send it to a second destination. |
iba AG - Data Acquisition and Analysis the way it should be |
|
This contribution was helpful to1 thankful Users |
Follow us on