7/23/2019 1:11 PM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
Hello for all. I would like to ask for some advices and help for solve my task. I need to send PDF file with report to a PC "shared" folder connected by network. i have read two manuals: How do you integrate an HMI operator panel into a local network? and What i made and it works: 1. Installed PDF creator 1.4 in the panel 2. Integrated TP700 into network with PC 3. I can save the report in PDF format at two destinations: Storage USB and PC (\\NOVA\LOGS) Now i need to send this repport from USB storage to another location at the PC. I used this code:
But it gives error code 424 (1A8) - the network path was not found. I tried also to use instead ip address the name of the PC like in settings of the PDF-printer. \\nova\logs. - but it also give the same error. I want to make two different buttons first for the print in PDF and save in USB and second for the saving in PC location. I made some error in the script or in the concept and it it not possible to send file directly by the script's commands? |
Last edited by: hadok at: 07/23/2019 13:12:05 |
|
Follow us on