7/25/2019 2:00 PM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Dear All, I would like to share an issue relating to Safety Signature and its solution. Problem: When I open the Edit Safety Program Dialog, print the signature, the file will always show "Program Changed", which is incorrect. Even I save the reference after full compilation and make a printout, it will show "program changed" as well. When I pressed compare, there are no difference and program showed Identical. After numerous tried, I found out there is some difference in the initial signature, highlighted in red colour, which was not shown in the printout. Attached with the pictures. Solution: From the DB number [1839], I found the instance data block in the chart. I deleted the blocks and added another one identical into it to trigger a change of instance block number. After triggering the change, I did a full AS compilation again. Then the red line in the "Edit Safety Program Dialog" disappeared. And the printout showed the correct "collective signature" instead of "program Changed" |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on