7/2/2019 9:51 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Dear Expert, Machine 10 axes HMC, configuration as below.
The machine is commissioned 6 months back & would like to take back up of Sinamics drives parameter via Starter. (I know it can be taken via START UP archieve.) I refered the related posts Connect to SINUMERIK / SINAMICS with STARTER - Entries - Forum ... &but not able to communicate with Sinamics drives with Starter & take a back up. I am able to go on line with PLC with ethernet & laptop so I donot think it is problem of cable or laptop settings. I have STARTER V4.5.1.0. Checked devices installed & found NCU list. NCU version is 4.07.35.84 where as machine NCU version is 4.07.04 (Photo attached) So my question is do I need to upgrade my STARTER software or missing something in STARTER communication setting parameters? Thanks in advance. DEEP. AttachmentAccessible nodes .zip (172 Downloads) |
7/2/2019 12:45 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Attched hardware configuration in Netpro for your ready reference. |
7/11/2019 6:20 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello ChristophD, Thank you very much for your reply. Since I was out of station delay in reply. I am connecting my Laptop with Sinumerik 840D SL NCU port ethernet port X127. In accessible nodes following are displayed -
To NCU 6 nos Sinamics S120 drives & to NX15 model 4 nos Sinamics S120 drives are connected.
NCU 720.3 PN has integrated SINAMICS CU which is inetrnally connected via PROFIBUS system, refere attached snap shot. Please check & reply. AttachmentHardware Confi.zip (170 Downloads) |
7/11/2019 7:48 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Yes, it is hardware configuration of PLC. Regards, DEEP. |
7/13/2019 5:31 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Anybody's suggestion/comment on subject issue! |
7/27/2019 6:57 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Does anybody has idea - how to access Sinamics drives via NCU ethernet port? |
Follow us on