7/28/2019 9:53 AM | |
Joined: 2/22/2008 Last visit: 5/10/2024 Posts: 2698 Rating: (206) |
The easiest way for this is a threshold trigger and an arithmetic block, see attached example. Maybe you want expand it with additional conditions like checking for lost connection, if possible. For this you must define the states for it, e.g. the zero is present for a longer time. The AI1 in the example is just for simulation. Regards, Scorp AttachmentHydroponic4.zip (199 Downloads) |
This contribution was helpful to1 thankful Users |
7/28/2019 8:23 PM | |
Posts: 20 Rating: (0) |
Today was a good day. Now all connected up and calibrated. I'm going for beer, cheers Scorp, ixo65 |
This contribution was helpful to1 thankful Users |
Follow us on