7/26/2019 9:16 AM | |
Joined: 6/14/2019 Last visit: 8/7/2021 Posts: 30 Rating: (1) |
TIA Portal V15.1, TP900 HMI, S7 1515 PLC Hi all,
For example, I will create some Text Fields or IO Fields, then connect the Style Item Appearance to one faceplate propert, and the Use Style / Design to another faceplate property. Sometimes when I do this, after saving, releasing the version of the faceplate and opening again, both the object properties are connected to both the faceplate properties. This seems like this could be a bug, or possibly user error on my part. Does anyone know why this is occurring and what I can do to prevent it? Example part 1: [snip] Example part 2: [snip] Thanks and regards, AttachmentExamples.zip (35 Downloads) |
Last edited by: Jen_Moderator at: 07/26/2019 12:27:40Removed links and added files as an attachment. |
|
Follow us on