7/25/2019 6:17 PM | |
Joined: 9/19/2009 Last visit: 9/21/2024 Posts: 459 Rating: (85) |
Hi What kind of drivers do you have in Wonderware? What are you talking about, Intouch or System Platform (Galaxy) Because, if you have installed, DAServer, then you can connect directly to WinCC. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
7/29/2019 10:14 PM | |
Joined: 9/19/2009 Last visit: 9/21/2024 Posts: 459 Rating: (85) |
Hi Sorry but still I don´t know if you want to access to the PLC or Tags from Intouch. If you only want tags from PLC , you have severals options. -If your PLC have ethernet, connect directly to WinCC -If your PLC don´t have ethernet, then you must use the OPC Server you have it, because WinCC support all types of OPC (OPC DA - OPC XML - OPC UA) So, if you want to read tags from Intouch ... If I don´t wrong, since version V.7 WinCC don´t support comunications DDE, because Intouch it is a server DDE. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on