8/2/2019 7:39 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi bt1060, by the PIDConL block the output PV_Out ist exactly the same value als PV. The output SP shows the active setpoint. So in your case you find at PV_Out the process value 34.8°C and at the output SP is the active setpoint 35°C (because SP_Ext := 35, SP_LiOp := 1, SP_ExtLi := 1). More Information about the inputs and outputs of the PIDConL block you can find in the manual PCS 7 Advanced Process Library at section PIDConL I/Os. With regards |
Last edited by: Heisenberg2 at: 08/05/2019 12:27:46 |
|
Follow us on