8/5/2019 11:53 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
I have a newly installed WinCC 7.4 Upd1 server (installed on a Windows server 2012 R2) that is going to replace the current WinCC 7.0 (installed on a Windows / PC). I have migrated the WinCC project (the project in VersionDog is integrated with both PLC logic and WinCC in the same Simatic Manager project) and would like to download it to the new server. However - even though I can ping the new server from the Engineering station Simatic manager cannot see the server (see attached screenshot). Could I just copy the WinCC project with my Windows explorer to the new destination (changed from C:\WinCC Projekt\KALEC01SERV01 to D:\WinCC\KALEC01SERV01? Should this new path be manually changed in the WinCC project or is it enough to "point" WinCC to the new location? Would I still be able to use our VersionDog setup (where we pull out a local copy of the project from the back-up server, make the changes we want - and save the modified project as a new version on the back-up server? AttachmentOMS.zip (46 Downloads) |
Last edited by: xmnj at: 08/06/2019 07:22:51Changed the headline |
|
Follow us on