8/3/2017 7:59 PM | |
Joined: 9/27/2006 Last visit: 5/9/2024 Posts: 12257 Rating: (2666) |
Hello Rescobedo; Besides not reaching your Festo module on the network, do you have any other symptoms or diagnostic messages? Do you have any diagnostic LED active on the CPU or the festo module? Did you go Online in the HWConfig editor to see if any module on the bus is declared as defective? Id any module is shown Online with a red slash icon, then its diagnostic buffer contains messages you should look at, by double-clicking on that error icon. What gsd file have you used to setup the Festo CPX-FB13 as a slave on your network? Does it correspond to this one: Hope this helps, Daniel Chartier |
8/9/2019 12:16 AM | |
Joined: 11/14/2016 Last visit: 8/22/2022 Posts: 2 Rating: (0) |
Facing Same Problem with same error code. Kindly tell me remedies. |
7/1/2023 10:27 AM | |
Joined: 1/27/2016 Last visit: 5/8/2024 Posts: 5 Rating: (0) |
image 2 |
This contribution was helpful to1 thankful Users |
Follow us on