8/8/2019 10:13 AM | |
Joined: 6/14/2019 Last visit: 8/7/2021 Posts: 30 Rating: (2) |
TIA Portal V15.1, 1515F PLC, TP900 Comfort HMI I am trying to execute a faceplate script using the ChangeValue event on a property of the faceplate. When I assign the property to an internal HMI tag which is set via a button on the HMI, the script will not execute. When I assign the property to a PLC tag which I manipulate manually, the script will execute. I've tried multiple HMI internal tags and multiple tags linked to the PLC, with the same result. Screenshots are attached.
Thanks and regards, Angus AttachmentFaceplate Script Problems.pdf (348 Downloads) |
Follow us on