8/10/2019 4:31 PM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following might help: 1-Compress the Memory Card ------------------------------------------------------------------- Compressing blocks: When data are compressed, gaps which have developed between memory objects in load memory/RAM as a result of load/delete operations will be eliminated. This releases free memory in a continuous block. Data compression is possible when the CPU is in RUN or in STOP. ------------------------------------------------------------------- 2-Save to Memory Card |
Eng.Mohamed Ibrahim |
|
Follow us on