8/13/2019 2:48 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Soroosh, Try Start Life List after connecting the Profibus PA devices in your loop. You can right-click on the DP/PA module, Profibus for checking the address in the loop. Before an instrument is set, the default of the address is 126. Let's say you have connected two default instruments in the loops, then in the life list, you will only see one device. See attached and hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on