8/14/2019 2:11 PM | |
Joined: 1/6/2019 Last visit: 12/6/2022 Posts: 21 Rating: (0) |
I changed something in project because level switch in V2 idea didn't work in aplication . Next I will attach a draw which shows two level sensors work status possibility and I hope that would be possible to rework project so in conclusion thist two level indicators low and hi will give at output 0 or 1 AttachmentWater valve control_FS4_V3.zip (173 Downloads) |
8/14/2019 2:13 PM | |
Joined: 1/6/2019 Last visit: 12/6/2022 Posts: 21 Rating: (0) |
level sensors status draw for project |
8/14/2019 3:21 PM | |
Joined: 1/6/2019 Last visit: 12/6/2022 Posts: 21 Rating: (0) |
you are right it is my mistake :should be L1=1 and L2=1 |
8/14/2019 4:32 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32875 Rating: (4064)
|
Then try this.
AttachmentWater valve control_FS4_V4.zip (182 Downloads) |
8/14/2019 9:11 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32875 Rating: (4064)
|
Version 5.
AttachmentWater valve control_FS4_V5.zip (210 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on