8/10/2019 8:59 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Which is MLFB number of PCU & system software version? |
8/10/2019 9:33 AM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
802D SW 02.01.05 MFLB 6FC5610-0BA10-0AA1 |
8/15/2019 8:54 PM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
Milling I can select axis A1 in the controller. How do I check MFLB ? |
11/6/2019 10:30 AM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
Hi again, Can I buy a LT module for like 2x15A and only use ONE servo drive inside it ? If so, how ? |
11/6/2019 12:50 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Yes, you can use but since you can add only 1, going for double module will be wastage of money.. In order to add 1 additional drive + motor, you need to configure its address, telegram type, encoder connections, motor data etc. etc. & need to tune additional axis. Please referSINUMERIK 802D: Turning, Milling diagnosis manual &802D: Turning, Milling commissioning manual &SINUMERIK 802D: Milling programing manual for more detail information. HTH |
Last edited by: Jen_Moderator at: 11/06/2019 12:52:47Optimized link. |
|
6/29/2020 4:32 PM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
So no changes is needed to the PLC program ? |
6/30/2020 9:57 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Have you referred manuals suggested in my earlier/previous post? |
Follow us on