9/2/2016 3:11 PM | |
Posts: 5 Rating: (0) |
Hello there! I have also a big problem with my Comfort panel. I have TP700 Comfort. V13 and Tia portal V11 with the latest update, but I have problem to get it work. I cant download OS V11 to the panel and it is the only OS i have. Can´t i use Tia V11 with TP700 comfort V13? Please help ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/5/2016 9:31:11 AMNew subject after splitting |
|
9/2/2016 3:13 PM | |
Posts: 5 Rating: (0) |
Another pic |
9/2/2016 4:04 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello Per_Cederholm, normally, ther should be an automatic downgrade of the panel image to V11 when downloading the project to the panel. You can also change the image on the oanel to V11 manually:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
9/3/2016 5:23 PM | |
Posts: 5 Rating: (0) |
|
Last edited by: Per_Cederholm at: 9/3/2016 5:29:50 PM |
|
8/14/2019 9:21 AM | |
Joined: 7/21/2015 Last visit: 2/14/2023 Posts: 1 Rating: (0) |
are you solved the problem please, because i have the same problem with tp900 |
Follow us on