8/20/2019 9:30 AM | |
Joined: 6/30/2015 Last visit: 10/5/2023 Posts: 31 Rating: (0) |
Dear find the attached picture. but it is not display plcsim |
8/20/2019 9:58 AM | |
Joined: 6/30/2015 Last visit: 10/5/2023 Posts: 31 Rating: (0) |
and while pressuring of switch to project view PLCsim is closing automatically. |
8/20/2019 10:02 AM | |
Joined: 6/30/2015 Last visit: 10/5/2023 Posts: 31 Rating: (0) |
dear sir, i did unstall and install two time but still same, and i ave attache set PG/PC setting also. |
8/20/2019 10:18 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
hello, is also plcsim V13 installed on the system or was installed in the past? Regards Christoph |
8/20/2019 10:28 AM | |
Joined: 6/30/2015 Last visit: 10/5/2023 Posts: 31 Rating: (0) |
yes sir, i have v13 and version 14 PLC sim both install on my computer. |
Follow us on