8/20/2019 8:16 PM | |
Posts: 7 Rating: (0) |
[snip] facing issue with PG/PC block monitoring online and downloding slave PLC Configuration details as following Rcoax wireless network consisting 6 Access Points (W 774-1 6GK5774-1FX00-0AA0) And 22 client (W 722-1 6GK1417-5AB10)+ IE/PB Link (6GK1 411-5AB10) Master PLC- CPU 317-2PN/DP Slave- IM151-7 quantity 22 Project Description- EMS ( 22 Moving nodes with PRB) Existing system running on PROFIBUS Master/Slave(with PRB) Configuration for EMS application. We are migrating Profibus Network to Profinet wireless system with using RCoax and IE/PB Link. 11 slave PLC profibus network migrated successfully on wireless profinet. Remaining 11 slave PLC's communicating on Profibus to master. for more details follow the link PLC Backup. Access Point setting- selected wireless configured with IPCF standard setting. Ipcf Cycle time-64ms HW retries-20 using channel-161,153,48,36,157,44 for 6 access points. Master PLC Profinet update time modified with 128ms. getting 100% communication result for master/slave profinet communication but unable to monitoring slave block online and download plc blocks. software- Step7 5.5 sp4 HF11 Please support for setting of profinet to get PG/PC online with slave plc. Thank You. Backup Link- [snip] ------------------------------------------------------------------------------------------ AttachmentCabems.zip (16 Downloads) |
Last edited by: Shubham_panghate at: 08/20/2019 20:22:14Last edited by: Shubham_panghate at: 08/20/2019 20:25:41Last edited by: Jen_Moderator at: 08/21/2019 09:22:35New subject after splitting. Division of questions into seperate topics. Deleted link and added file as an attachment. |
|
Follow us on