8/21/2019 4:15 AM | |
Posts: 1 Rating: (0) |
Hi I am converting the V13 Backup to V15 Error Occured.please sea the below error. Error: The project includes instruction profiles. Delete all instruction profiles. If necessary, create new instruction profiles after the migration. 8/13/2019 4:44:29 PM Error occurred while converting the type 'CodeBlockData' (model type 'Siemens.Simatic.Lang.Model.Blocks.CodeBlockData') 8/13/2019 4:44:31 PM Unconverted object type found: 'Object' (Model type 'Siemens.Simatic.AlarmServices.Model.LangConnector.AlarmServicesDataContainer') 8/13/2019 4:44:32 PM Unconverted object type found: 'Object' (Model type 'Siemens.Simatic.FPlus.FEngine.Interface.Model.FailsafeInfo') 8/13/2019 4:44:32 PM Unconverted object type found: 'Object' (Model type 'Siemens.Simatic.Hmi.Utah.Common.Base.HmiConvertData') 8/13/2019 4:44:32 PM Unconverted object type found: 'CodeBlockData' (Model type 'Siemens.Simatic.Lang.Model.Blocks.CodeBlockData') 8/13/2019 4:44:32 PM The project or library possibly contains data that cannot be upgraded by the currently installed software. Repeat the upgrade with a newer version of your software that includes more functionality. 8/13/2019 4:44:32 PM Upgrade failed. For more information, see the log file. If the project still cannot be upgraded. please contact Siemens Customer Support. 8/13/2019 4:44:32 ------------------------------------------------------------------------------------------ AttachmentV13 to V15_Migration_Log.pdf (543 Downloads) |
Last edited by: Jen_Moderator at: 08/21/2019 10:27:13New subject after splitting |
|
7/2/2021 2:09 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi, Did you first converted it to V13 SP1(or SP2) an compiled it? When you want to upgrade your project to V14 or higher, the project needs to be compiled with at least V13 SP1. The latest version of V13 is SP2 Upd4 and can be downloaded here: SIMATIC STEP 7 inkl. PLCSIM V13 SP2 TRIAL Downloadif this doesn´t help, read the information that you gave us: "For more information, see the log file." hope this helps, regards, |
FCK WAR! |
|
Follow us on