8/21/2019 9:21 AM | |
Posts: 21 Rating: (0) |
Greetings, I have a problem with my connection between WINCC V7.4 and S71500, my questions are: 1) I already follow instructions from Siemens but still having a problem which is status disconnected. what would be the problem? 2) Is my hardware config in TIA correct? AttachmentWinCC74_1500.pdf (141 Downloads) |
8/21/2019 9:22 AM | |
Posts: 21 Rating: (0) |
This is my connection status |
8/21/2019 9:23 AM | |
Posts: 21 Rating: (0) |
This is my connection parameter |
8/21/2019 9:24 AM | |
Posts: 21 Rating: (0) |
This is my hardware config in TIA. Please help,thank you! |
8/21/2019 9:28 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
Can you give a screenshot of "Set PG / PC interface"? |
8/21/2019 9:32 AM | |
Posts: 21 Rating: (0) |
These are software's installed in my PC |
8/21/2019 9:34 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
This is available from the Windows control panel. As in the instructions from the first post. |
8/21/2019 9:35 AM | |
Posts: 21 Rating: (0) |
My PGPC |
Follow us on