8/22/2019 6:50 PM | |
Posts: 17 Rating: (0) |
Hallo Guys, I am new in plc world and finding diffculties in cyclic execution of code. I have made fb and calling in main OB1. The code starts motor and that goes in one direction and then in other direction and stops. I want to run continuously instead of only one time. Please help me in this regard. Anylead willlbe help full. Note: Tag "blockntw" and "disable power" are defined as stats with default value 0. ------------------------------------------------------------------------------------------ AttachmentTO_Siemens.pdf (142 Downloads) |
Last edited by: Jen_Moderator at: 08/23/2019 06:59:26New subject after splitting |
|
8/23/2019 9:40 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804) |
Hello further on, there are a lot of helpful applications (easy in use) on siemens support available https://support.industry.siemens.com/cs/ww/en/view/109749348 for example : Motion via LAxisControl read/write drive parameter, TimeSynchronisation … via LAcycCom |
With best regards, |
|
This contribution was helpful to1 thankful Users |
8/23/2019 3:18 PM | |
Posts: 17 Rating: (0) |
Hallo jacek d, The code is attached here AttachmentTO_Siemens (FB3).pdf (127 Downloads) |
Follow us on