8/22/2019 11:24 PM | |
Joined: 1/15/2019 Last visit: 10/27/2021 Posts: 16 Rating: (0) |
Hi guys, I`d like to connect many different stations via SHDSL/IEC 60870-5 protocol like seeing in attached file (it`s important to provide redundancy at DSL link level). Would this configuration work in practice? What is the maximum range (in km) between two SHDSL modems at 0,6 mm2 twisted pair? What should I take into account to prevent loop? I read somewhere that helps using different VLANs at ethernet and DSL networks. Any idea or experience? Thanks in advance, Banchy ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/23/2019 10:43:26New subject after splitting |
|
Follow us on