2/22/2019 6:08 AM | |
Joined: 2/23/2016 Last visit: 2/14/2024 Posts: 36 Rating: (2) |
Hi I am using PCS7 and insert an Channel driver only and connect to input.but when i turn on input (I0.0), value of CH_Di change to 1 .but Q stay in 0 condition. Can you help me??? Regards. mojtaba fathi ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 2/22/2019 1:27:31 PMNew subject after splitting |
|
8/23/2019 11:39 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
This refers to the block calling sequence. If the sequence is incorrect, this symbol is displayed. If the sequence is incorrect, the program will work, but there will be a slight delay in the signal transmission between the blocks. You can try to fix this automatically (Options -> Optimize Run Sequence). Attachments7cfcs7b_176.pdf (126 Downloads) |
Follow us on