7/31/2019 11:59 AM | |
Joined: 2/21/2016 Last visit: 8/3/2022 Posts: 3 Rating: (0) |
Kaulquappe, I'm facing problems with 502 port in 6GK7443-1EX20-0XE0 FW 2.0 through a Modbus TCP connection. In our drive log appears error 10061. Sometimes changing CPU status (Run => Stop => Run) solves the problem. But sometimes doesnt. Do you recommend upload the firmware? Best Regards! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/31/2019 13:51:38New subject after splitting |
|
8/13/2019 3:24 PM | |
Joined: 3/21/2018 Last visit: 2/17/2022 Posts: 5 Rating: (0) |
Try to use port 102 and check. |
8/26/2019 2:10 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, hope not here on MB/TCP (Port 102)... |
With best regards... |
|
Follow us on