6/27/2019 3:19 PM | |
Joined: 4/14/2010 Last visit: 3/27/2024 Posts: 523 Rating: (11) |
Greeting, Looking for the selection of SINAMICS S210 with power range 0.1kW to 7kW But unable to find in Online DT Configurator and SIZER for Siemens V3.20. (attached) any alternative source for the selection including data sheets, dimension, 3D/2D drawings. Manual released April 2019.
AttachmentSizer & DT.zip (203 Downloads) |
MS |
|
6/28/2019 6:55 AM | |
Joined: 2/7/2018 Last visit: 3/14/2023 Posts: 181 Rating: (30)
|
Hello, You will find data sheets, dimensions, 3D/2D drawings in “Documents” placed in the DT-Configurator (see screenshot attached). The SINAMICS S210 drive system is also included in the TIA Selection Tool (offline Version). https://new.siemens.com/global/en/products/automation/topic-areas/tia/tia-selection-tool.html Best Regards, |
6/28/2019 9:46 AM | |
Joined: 4/14/2010 Last visit: 3/27/2024 Posts: 523 Rating: (11) |
Thank You! TechSupport SINAMICS S210 We are Looking for the Selection of S210 drive and 1FK2 servo with Power 1.3KW Voltage 400V Ampere 10.7A Speed r/min 1500 and Torque Nm 8.34 Which is not configurable in DT, Sizer and as well TST. (attached) but available in manual page 34 & page 53 Catalog_D32-SINAMICS_S210_Servo_drive_system.pdf Converter 6SL3210-5HE11-5UF0 Motor 1FK2 . 06 Shaft height 63 AttachmentS210.zip (88 Downloads) |
MS |
|
6/28/2019 1:00 PM | |
Joined: 4/14/2010 Last visit: 3/27/2024 Posts: 523 Rating: (11) |
Thank You! TechSupport SINAMICS S210 We require OCC for S210, when we select the this option the DT doesn't display any option for 12Nm (attached) https://mall.industry.siemens.com/mall/en/WW/Catalog/Product/1FK2206-4AF01-1SB0 1FK2206-4AF01-1SB0 SIMOTICS S-1FK2 CT Servo motor M0=12 Nm; PN = 2.9 kW at nN=3000 rpm; Converter at max. 480 V supply system; Degree of protection IP65; Shaft D24x50 mm with fitted key; Absolute value encoder singleturn 22-bit (encoder AS22DQC); With DRIVE-CLiQ interface; Power connector Size M23 Above 1FK2 servo motor 2.9kw 12 Nm is for S120 drive with double cable connection DRIVE-CLiQ interface. While New S210 drive is supported for one cable solution MOTION CONNECT 500 6FX5002-8QN04-1AE0 Connector size M12. |
Last edited by: MS1981 at: 06/28/2019 13:01:24MS |
|
6/28/2019 2:22 PM | |
Joined: 2/7/2018 Last visit: 3/14/2023 Posts: 181 Rating: (30)
|
Okay, i will check this. Best Regards, Technical Support S210 |
7/5/2019 2:08 PM | |
Joined: 2/7/2018 Last visit: 3/14/2023 Posts: 181 Rating: (30)
|
The release is planed for Q3 2019. Best Regards, Technical Support S210 |
Follow us on