11/19/2008 7:35 AM | |
Posts: 116 Rating: (1) |
I think there GSD file comes with there software. Just check there software regards Paresh |
11/19/2008 7:51 AM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979) |
Hello, download it from www.lenze.com Regards Christoph |
11/19/2008 8:09 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello Link:GSD/GSE files for Lenze profibus-DP communication modules (Software installation: regards |
11/19/2008 8:01 PM | |
Posts: 137 Rating: (1) |
Hi i'll check your file thanks for your information maher |
8/31/2019 9:09 AM | |
Joined: 6/14/2015 Last visit: 3/26/2024 Posts: 236 Rating: (1) |
thanks so much. but your link is dead. you can find GSD and GSDML for all products of LENZE in this link. https://www.lenze.com/en-de/services/software-downloads/engineering-data/ |
This contribution was helpful to1 thankful Users |
10/16/2020 8:31 PM | |
Posts: 3 Rating: (1) |
Hi.when i uploaded program for backup , came this error message . |
10/16/2020 9:01 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665) |
Hello Registration; You receive this message because you are trying to link your CPU to a Profinet IO Device on an uploaded project. The GSDML files are not installed on the CPU, but on the programming PC, so they cannot be uploaded from the CPU project. The answer is that you must go to the Lenze website, locate that specific GSDML file, download it to your computer and install in in your Step 7 software. The error message should disappear.once the program is compiled and downloaded to the CPU. This note can be found on the webppage for the "GSDML device description files for Lenze Profinet IO devices" (where you can download a zip file with all Lenze GSDML files). https://www.lenze.com/en-de/application-knowledge-base/article/200804173/1/ 8400 Motec Note: Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/16/2020 21:44:10Last edited by: dchartier at: 10/16/2020 22:05:45 |
|
10/17/2020 2:51 PM | |
Posts: 3 Rating: (1) |
I downloaded 2015 and 2016 versions of xml but it didn't help. It says that version 2.02 and higher. But that's not true |
Follow us on