8/29/2019 8:20 PM | |
Joined: 9/27/2006 Last visit: 5/13/2024 Posts: 12257 Rating: (2667) |
Hello mpvel; What error messages do you receive when you configure your DP/DP coupler? What are the contents of the diagnostic buffer that you can link to this DP/DP coupler? Has the coupler.s second slave interface been configured on a separate Profibus-DP master? Dis you setup the data exchange areas so they are the opposite (same data size, inputs for the first master become outputs on the second master) in the 2 masters individual Profibus configuration? What are the special features of input/output addressing with the DP/DP coupler? https://support.industry.siemens.com/cs/ww/en/view/22327981 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
8/30/2019 6:50 AM | |
Joined: 1/28/2019 Last visit: 7/11/2023 Posts: 6 Rating: (0) |
Sir, i was getting error in coupler SF1 , SF2 led on condition and BF1, BF2 led flash conditionin software we got in error HW not found in tiav15 in our configuration between s7 - 300 data exchange between DCS both device are master our coupler act like slave . |
8/30/2019 8:20 AM | |
Joined: 1/28/2019 Last visit: 7/11/2023 Posts: 6 Rating: (0) |
Sir my conguration are attched here pls refer sir AttachmentS7 -300 WITH DP_DP ERROR.xlsx (204 Downloads) |
Follow us on