7/29/2019 4:22 PM | |
Posts: 3 Rating: (0) |
I have the similar problem. What should I do? Could you help me please? ERROR:You are attempting to change the counter value '"indexes10"' of a FOR loop. tia v14 FOR "indexes10" := "T8_Yatay_eksen_giriş_offset_değeri_Array" TO "T8_Yatay_eksen_çıkış_offset_değeri_Array" BY 1 DO IF ("MATRİS_Yatay_eksen".FBB_Matrisi_B2["indexes10"] <= "MATRİS_Yatay_eksen".FBB_En_küçük_degeri_B2[8]) AND ("MATRİS_Yatay_eksen".FBB_Matrisi_B2["indexes10"] <> 0) THEN "MATRİS_Yatay_eksen".FBB_En_küçük_degeri_B2[8] := "MATRİS_Yatay_eksen".FBB_Matrisi_B2["indexes10"]; ; END_IF; IF ("indexes10" = "T8_Yatay_eksen_çıkış_offset_değeri_Array") THEN "indexes10" := "T8_Yatay_eksen_giriş_offset_değeri_Array"; ; END_IF; ; END_FOR; ------------------------------------------------------------------------------------------ |
Last edited by: mkeeng at: 07/29/2019 16:25:18Last edited by: Jen_Moderator at: 07/30/2019 12:50:24New subject after splitting |
|
This contribution was helpful to1 thankful Users |
Follow us on