9/5/2019 7:35 PM | |
Joined: 9/17/2015 Last visit: 10/4/2023 Posts: 137 Rating: (4) |
Hie all, I am trying to implement traffic light logic in TIA v14 using Graph sequential programming. I was able to add a TP(Time pulse time) and turn it on with a bit m0.0. The instruction or the Elapse time of the timer should reset when m0.0 goes to zero. Once the cycle is completed (green->yellow->red) I am resetting the bit but with this reset non of the timer are resetting to zero. Can anyone guide me and suggest me correction. Please feel free to ask question. Attachmentimages.zip (88 Downloads) |
9/5/2019 10:15 PM | |
Joined: 9/17/2015 Last visit: 10/4/2023 Posts: 137 Rating: (4) |
Thanks a lot , there is very little help available for Graph programming. your answer fulfils my requirements. |
Follow us on