7/25/2019 4:36 PM | |
Posts: 3 Rating: (0) |
Hi, need some help for solar panel program (attached). I need to compare temperature between solar panel PT100 (B017) and hot water tank PT100 (B001) to activate solar panel pump (Q7) only in this condition: - Temperature of solar PT100 must be 5°C higher than tank PT100 Thanks all Attachmentfra.zip (239 Downloads) |
7/25/2019 4:55 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33798 Rating: (4199)
|
Hello franc82, at first welcome to the forum. Attached the modified diagram. If the solar Pt temperature is 5 °C higher than the other Pt temperature, the solar pump will be switched on. If the temperature difference drops to 3 °C or less, the solar pump switched off. Attachmentfra_V2.zip (291 Downloads) |
This contribution was helpful to2 thankful Users |
7/29/2019 10:52 AM | |
Posts: 3 Rating: (0) |
Good morning, program works well Thank you very much |
This contribution was helpful to2 thankful Users |
Follow us on