9/9/2019 3:43 PM | |
Joined: 8/27/2019 Last visit: 5/2/2024 Posts: 3 Rating: (0) |
Hi to everybody, I'm trying to use a CPU 1512SP F-1 PN (6ES7 512-1SK01-0AB0) and a CM PtP board (6ES7 137-6AA00-0BA0) to communicate with a Siemens V20 via USS. I'm using TIA Portal V15.1. I used exactly the same example available at the following link: https://support.industry.siemens.com/cs/it/it/view/90468030/en but I'm not able to start the connection, I continue to get error code 8281 on USS_Port_Scan: Siemens help says to check PORT parameter, but it's already set to the correct hardware ID of the board. I tryed to change some settings inside the hardware configuration of the CM but without success. I set-up the V20 as described in the example guide: I'm not getting any F72 fault code even if the communication cable is disconnected, isn't it strange? Does anyone know what to check first? |
Last edited by: Jen_Moderator at: 09/10/2019 09:02:46Optimized link. |
|
Follow us on