9/10/2019 1:42 PM | |
Joined: 9/23/2013 Last visit: 4/18/2024 Posts: 46 Rating: (0) |
Dear sir, I have a one confusion.I have to migrate total 4 nos of master drives to sinamics S120.I have studied old simovert master drive mc back up and found wide complex logic. I want know something about simovert master drive mc v/s S120 parameter settings. (1)As per Master drive MC P169=1 & P170=82690264.That means AVWF=1.82690264 .Both parameters are sets for AVWF(Actual value weighting factor) Please share your knowledge to which parameters have to set in S120 against the P169 & P170. (2)How to set LU per load revolution.We already know that default value is P2506=10000(Lu per load revolution(pos.stpt/act val resolution)==?????? Note:I have to set P2506 (Lu per load revolution(pos.stpt/act val resolution)as per master drive back up.Can please suggest the parameter in master drive mc? Cu320-2 DP Sinamics S120 Motor :1FK7080-2AF71-1SH0 ,3000 rpm,multipole resolver. Gearbox :Ratio :1400/104 Application : belt for used for glass movement. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/11/2019 08:56:26New subject after splitting |
|
Follow us on