9/11/2019 7:57 PM | |
Joined: 2/1/2010 Last visit: 9/19/2024 Posts: 150 Rating: (71) |
I have only ever done it according to the manual passing through an EventTs or EventTs16 block. You can see the example in CFC in the provided Motor_AV_EventTS template of the APL library. You could pass it through on to a MonDiL instead of MotL afterwards. If you look at the structure of the TS_Out on the Pcs7DiIT block vs the structure of EventTsOut on the EvenTs block, they are not the same. I think you can't shortcut it, otherwise the input EventTsIn input doesn't get the right data and the message doesn't generate correctly. The inputs are ANY type, so you won't get an interconnection error. I'm interested if you find in testing that it works without the EventTs block, but I don't think it will. |
Last edited by: RVS.wick at: 09/11/2019 19:57:27Last edited by: RVS.wick at: 09/11/2019 19:58:33If my post helped you, please rate. Thanks. |
|
Follow us on