9/12/2019 7:04 PM | |
Joined: 10/4/2017 Last visit: 3/30/2024 Posts: 4 Rating: (0) |
Hi all, I have been asked to provide an OPC connection from WinCC 7.0 to an external system, to be able to transfer variables from the WinCC SCADA system for further processing on a separate system. From what I gather this should be easy enough with WinCC.OPC Server... or so I thought The OPC client for the aforesaid external system has not been selected yet, but I set off to prove the operation of the WinCC OPC server. On the same PC with the WinCC Runtime I tried using the OPC Scout, resulting in an error. I have read through "WinCC V7.0 SP2 OPC - Open Connectivity" and various support topics but I don't have the brain capacity to utilise that information to get a healthy WinCC OPC Server - OPC Scout/Client relationship going. I kindly ask if any of you experts would be able to review the snapshots included and maybe point me in the right direction. Best regards, AttachmentwinCC_OPC_Server.zip (45 Downloads) |
Follow us on