10/9/2017 4:42 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (267) |
It is seem like a software bug to me. 1. have u checked your archive destination? Any folder permission setting ? ( just check for fun) 2. what is your WinCC, and Batch version? May be Siemens released the update version for your Simatic Batch? you may search and see. 3. Ultimate: Send a Support Request https://support.industry.siemens.com/cs/ww/en/sc/2100 Attached my installed software for V8.2. (dun have Batch V8.2) for your comparison. AttachmentProducts.zip (106 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
10/10/2017 3:54 PM | |
Posts: 5 Rating: (0) |
Hi Jaz, I have never seen this before. 1. Yes. It gone through. Also, I have set the "waiting time after closing" in the Project Setting -> Close and Archive into 0 2. PCS7 V8.2. I do not apply the update version. Will consider it. 3. Sound's like a plan.. * Additional Info: The stations are OS redundant whereby Batch Server is also OS server. No Batch Redundant. It is using VM in Domain Network. Thanks, TTK |
10/10/2017 5:09 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (267) |
2. keep your software update can solve quite a lot of problems. If any updates u cannot find online, but my version is more updated, let me know, i can pass u the update. 3. yea, that is the best way for this type of problems. It really seem like a bugs more than configuration error to me. 4. ""* Additional Info: The stations are OS redundant whereby Batch Server is also OS server. No Batch Redundant. It is using VM in Domain Network."" even in domain network, as long as u are using the same user name, then read / write documents no issue, i dont think it will cause problem. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
9/14/2019 4:26 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (267) |
Thank you for sharing |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on