9/15/2019 12:11 AM | |
Joined: 9/14/2019 Last visit: 6/1/2023 Posts: 16 Rating: (0) |
i asked if i can access to starter through MPI PLC connection (routing) s7 300 |
9/15/2019 5:39 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Which device you want to access via STARTER on MPI? Drive - yes. PLC - No. |
9/16/2019 10:05 AM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328) |
The drives must be under the S7-CPU in SIMATIC Manager. If they are on the same level as the S7-CPU you need Drive ES. Then setup the routing: https://support.industry.siemens.com/cs/ww/en/view/2383206 In Starter you have to change the online interface to S7 (not DRIVE). |
|
|
This contribution was helpful to1 thankful Users |
9/16/2019 8:47 PM | |
Joined: 9/14/2019 Last visit: 6/1/2023 Posts: 16 Rating: (0) |
thanks in advance it's really useful link,i will try it and revert with feedback |
9/29/2019 10:31 AM | |
Joined: 9/14/2019 Last visit: 6/1/2023 Posts: 16 Rating: (0) |
other photo |
Follow us on