9/17/2019 9:29 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
You can use SFB3 - SFB5 timers by creating instance data block for timers (link). Then there is no need to create a DB for each timer. Also in PCS, FBs are often called from OB3x cyclic interrupts. At the input of FB, you can provide the input SampleTime - the period of the call. Then, to calculate the time, you can simply summarize this value and save it in a variable in the "static" area. |
9/17/2019 1:33 PM | |
Joined: 8/19/2017 Last visit: 4/24/2024 Posts: 79 Rating: (3) |
That's exactly what I want, Thanks |
Follow us on