8/29/2019 9:15 AM | |
Joined: 10/24/2012 Last visit: 3/8/2024 Posts: 307 Rating: (21) |
Dear Experts, We have two WINCC explorer system running with a CPU 412 H redundant system.One day one of the WINCC stuck during the RT and when we close it and try to open it again it didn't run and stuck and loading on 68% . I uninstalled the WINCC RT and try to reinstall it and during the installation of the WINCC Explorer Asia version 7.3. During installation i received the messages of entry point not found and after completing the installation the WINCC explorer runs but couldn't able to open any project and gave the same error of entry point not found. Pictures are attached for your reference. Thanks in advance. Kashir Saeed. AttachmentWINCC Pics.zip (46 Downloads) |
Kashir Saeed. |
|
9/18/2019 3:24 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hi, in this case I would recommend to create a service request and send the SDT data to the technical support: https://support.industry.siemens.com/cs/ww/en/sc/2090 Regards |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on