9/17/2019 12:42 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, have a look at the Masterdrives Vector Control Compendium and there to function diagram 481. With U821 to U834 you can set up 4 speed thresholds (in %) with a common hysteresis of U836, and use the feedback signals in the corresponding binectors B0851 to B0854 as source for your digital outputs. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
9/18/2019 12:18 PM | |
Joined: 9/12/2019 Last visit: 1/22/2023 Posts: 3 Rating: (0) |
Thanks for your reply.I tried to set these parameters. If you set the parameter P653 binector B853 then the output is always activated and does not switch to 0 if V> V3. In the attached file, Vact> V3 but the output is triggered (+ 22V). What could be the problem? |
Follow us on