9/22/2019 7:57 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello Boosted6, Alarm 300608 is - speed controller at its limit. Since you have checked related points, I suggest you to check below points. 1. Does this alarm trigers at particular area? If yes check axis mechanic at that particular area. 2. Check DC link volatage during/when this alarm trigers. 3. Check MD1605 & MD 1606 values. 4. Check MD 1105 value. Corelate this value with motor LT power module & motor nameplate detail. HTH. |
Last edited by: PISCEAN 2010 at: 09/22/2019 07:59:16 |
|
9/23/2019 1:49 PM | |
Posts: 672 Rating: (56) |
Hi, Is the axis actually moving?. It sounds to me like there is only precharge on the DC bus. What is the DC bus voltage reading?. Pee |
Follow us on