9/23/2019 6:38 PM | |
Joined: 10/24/2012 Last visit: 3/8/2024 Posts: 307 Rating: (21) |
Dear Experts, I am trying to implement the SIEMENS provided example of "Programming an OPC UA .NET client with C# for the SIMATIC NET OPC UA Server". Everything works fine until i tried to connect the server with the provided C# application. I opened the application OPC UA simple client and entered the URL of my server as highlighted in the attached screenshots. and when i entered it, it gives me the error "Invalid URI: invalid port specified" and now i am stuck at this point, another thing in the provided manual on address https://support.industry.siemens.com/cs/ww/en/view/42014088 the server is not secured while my server is secured and also my server is opening port 55101.Can anyone guide me where is the fault and why i am not able to make the connection. Thanks in advance. AttachmentOPC_UA.zip (56 Downloads) |
Last edited by: Kashir at: 09/23/2019 18:40:14Last edited by: The Helping Hand at: 09/24/2019 14:48:55Optimized Link. Kashir Saeed. |
|
Follow us on