9/6/2019 2:05 PM | |
Joined: 4/10/2006 Last visit: 5/4/2024 Posts: 901 Rating: (2) |
Hi another question: with the ESC key I can no longer access the SIEMENS M6 PG bios ... something will have failed I asked for the possibility to reinstall the bios and I managed to download it from your site ... I prepared the usb key but to start the bios from the usb key I have to enter the bios ... maybe I don't explained myself ! ! IN THE BIOS OF THIS PG IT IS NO POSSIBLE TO ENTRY ... WHEN I PRESS ESC THE SIEMENS LOGO APPEARS AND STOPS ... I can start windows ... it is not possible to make a usb key with the BIOS to boot from windows ??? These are the siemens instructions for installing the bios: --------------------------------------------------------------------------- (1) Instructions on running the BIOS update --------------------------------------------------------------------------- Preparation ----------- You need a USB stick with approx. 100 MB of available memory for the BIOS update. The USB stick must be FAT32 formatted but not bootable. Process ------- The following description assumes that the device on which you want to run the BIOS update is also used to prepare the required USB stick. 1. Do not switch off the IPC during the entire update process! 2. Unzip the BIOS ZIP file into a blank or newly created directory on your hard disk. 3. Start the unzipped EXE file. 4. Insert the USB stick into an available USB interface of the IPC and start the "EFIBIOS2USB.EXE" program. 5. (Optional) Logo replacement: Copy the OEM logo (400x300 pixels) to the BIOS folder on the USB stick under the name "Logo.jpg". 6. Restart the IPC. 7. Use the ESC button in the course of the boot phase to open the BIOS startup screen. 8. If there is no FAT formatted partition on a boot device (or no boot device), enter the BIOS Setup Utility and set "Boot -> USB Boot" to "Enabled". Restart the IPC. Use the ESC button in the course of the boot phase to open the BIOS startup screen. 9. Select the "BIOS Update" function in the BIOS startup screen. 10. Accept the BitLocker warning and the disclaimer and start the update process with "Y". --------------------------------------------------------------------------- can any PG M6 expert help me? thank you Roby ------------------------------------------------------------------------------------------ |
Last edited by: Roby at: 09/07/2019 02:23:57Last edited by: Jen_Moderator at: 09/09/2019 09:47:05New subject after splitting Setting of my PG M6 Siemens |
|
8/18/2020 3:49 PM | |
Joined: 3/23/2018 Last visit: 4/23/2024 Posts: 6 Rating: (0) |
Dear Roby, Have you found a solution? I have the same problem. Best Regards, Vilius |
Follow us on