6/2/2014 2:16 PM | |
Posts: 140 Rating: (7) |
Hello Manju, Have you enabled SFS Visualization option while OS compile? Best of Luck |
6/2/2014 3:12 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Have you checked the operator permissions? Operator can be enabled to use the buttons like "Start", "Abort" , "Stop". Each button can be set with authorization if operator is allowed to press it. |
If I could help you, you can use the RATE button. Thank you. |
|
9/26/2019 3:30 PM | |
Joined: 6/13/2016 Last visit: 7/23/2024 Posts: 17 Rating: (1) |
Hi all, I had the same problem in PCS7 v9. I recreated an SFC type and it work normal. |
Follow us on