9/27/2019 9:26 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (374)
|
Hi, You cannot read out the program alarms directly. What you can do is to use the FB "Get_Alarm" to write the program alarms into a datablock and read out the data then from this datablock with a S7 connection from the IOT2000. Here is an application example how to deal with "Get_Alarm". Have a look at the "documentation basics Get_Alarm". You won't need the part "sending alarm to PLC_2" in this application example because you will do this with the IOT2000 using a S7 connection. Are you aware of using S7 connection with IOT either in node-red or C/C++? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on