9/29/2019 6:44 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello Avatar; Below you will find a description of the 2 safety modules you are planning to use. These are Safety modules (recognizable by the yellow band in the front of the modules;).This shade of yellow is internationally recognized as indicating a Safety module or equipment. To integrate these modules as part of a Safety design, as per ISO 13849-1 (PLa to PLe) or IEC 61508 (SIL 1 to SIL 3), you must first have a Safety PLC, such as a S7-315F-2PN/DP; you msut also have an additional software package named Distributed Safety (for Simatic Manager) or S7-Safety v.1x (for TIA Portal). And you must have done a Safety design to determine the safety level you want to achieve, based on the standards mentionned above.See the following documents: SIMATIC Automation System S7-300 ET 200M Distributed I/O Device Fail-safe signal modules https://support.industry.siemens.com/cs/us/en/view/19026151 SIMATIC Industrial Software Safety Engineering in SIMATIC S7 https://support.industry.siemens.com/cs/ww/en/view/12490443 If you maintain the use of your S7-315-2PN/DP (not a Safety PLC) you can use your modules in a non-safety application, as regular I/O modules. Safety Light Curtains have specialized dual outputs that must be connected to a Safety Input module; these OSSD signals must be evaluated in the Safety module for "discrepancy" (there is a very limited amount of time where both signals must match when an intrusion is declared) or monitoring their response to pulse tests done in the Safety module.. This cannot be achieved with a non-safety input module. See for example page 12 &all. of this document from Rockwell for more details: https://literature.rockwellautomation.com/idc/groups/literature/documents/at/safety-at065_-en-e.pdf Hope this helps, |
Last edited by: dchartier at: 09/29/2019 19:01:12Last edited by: dchartier at: 09/30/2019 12:36:30 |
|
This contribution was helpful to1 thankful Users |
Follow us on